Extend Backplane Power Across the System
Each PointMax adapter and expansion power has MP connections. The input to these
connections are SELV 24V DC nominal.
Each adapter and expansion power uses MP to generate backplane power through an isolated
DC-DC convertor, sufficient to power 16 I/O modules and mounting bases.
The expansion power (5034-EXP or 5034-EXPXT) extends power on the rack beyond 16 I/O
modules.
Provide Feedback