Install System Components

When you build an
EtherNet/IP
In-cabinet system, the following must be completed:
  1. Prepare the panel.
  2. Lay out all hardware.
  3. Install the DIN rail and cable routing systems.
  4. Mount the
    EtherNet/IP
    In-cabinet system devices.
  5. Install the control hardware, including the gateway, supplemental power tap (optional), cable connector assemblies, controller, and power supply.
  6. Connect the Ethernet cable to the controller, gateway, Ethernet switch, and other standard
    EtherNet/IP
    devices.
  7. Connect the 1486-CBL flat media cable from the gateway to all other
    EtherNet/IP
    In-cabinet devices and include the end node terminator (1486-CON-T1).
  8. Complete the control wiring and power wiring.
  9. Check and tighten all connections.
  10. Apply power to the system. The gateway automatically assigns the IP addresses of node devices.
  11. Complete system configuration in a
    Logix 5000®
    controller project
ATTENTION:
Prevent Electrostatic Discharge
This equipment is sensitive to electrostatic discharge, which can cause internal damage and affect normal operation. Follow these guidelines when you handle this equipment:
  • Touch a grounded object to discharge potential static.
  • Wear an approved grounding wriststrap.
  • Do not touch connectors or pins on component boards.
  • Do not touch circuit components inside the equipment.
  • Use a static-safe workstation, if available.
  • Store the equipment in appropriate static-safe packaging when not in use.
ATTENTION:
Environment and Enclosure
This equipment is intended for use in a Pollution Degree 2 industrial environment, in overvoltage Category II applications (as defined in EN/IEC 60664-1), at altitudes up to 2000 m (6562 ft) without derating. This equipment is not intended for use in residential environments and may not provide adequate protection to radio communication services in such environments. This equipment is supplied as open-type equipment for indoor use. It must be mounted within an enclosure that is suitably designed for those specific environmental conditions that are present and appropriately designed to help prevent personal injury resulting from accessibility to live parts. The enclosure must have suitable flame-retardant properties to prevent or minimize the spread of flame, complying with a flame spread rating of 5VA or be approved for the application if nonmetallic. The interior of the enclosure must be accessible only by the use of a tool. Subsequent sections of this publication may contain more information regarding specific enclosure type ratings that are required to comply with certain product safety certifications. In addition to this publication, see the following:
  • Industrial Automation Wiring and Grounding Guidelines, publication 1770-4.1, for more installation requirements.
  • NEMA Standard 250 and EN/IEC 60529, as applicable, for explanations of the degrees of protection provided by enclosures.
ATTENTION:
This product, which is supplied as open-type equipment, must be mounted:
  • Within an enclosure that is suitably designed for those specific environmental conditions that will be present and appropriately designed to prevent personal injury resulting from accessibility to live parts. The enclosure must have suitable flame-retardant properties to prevent or minimize the spread of flame, complying with a flame spread rating of 5VA or be approved for the application if nonmetallic. The interior of the enclosure must be accessible only by the use of a tool. Subsequent sections of this publication may contain additional information regarding specific enclosure type ratings that are required to comply with certain product safety certifications. The enclosure must be accessible only by the use of a tool.
  • In an UKEX/ATEX/IECEx/INMETRO Zone 2 certified enclosure with a minimum ingress protection rating of at least IP54 (in accordance with EN/IEC/ABNT NBR 60079-0) and used in an environment of not more than Pollution Degree 2 (as defined in EN/IEC 60664-1) when applied in Zone 2 environments. In addition to this publication, see: NEMA 250 and IEC 60529, as applicable, for explanations of the degrees of protection provided by enclosures.
WARNING:
Installation Precautions
These products must only be:
  • Used as a component in an
    EtherNet/IP
    In-cabinet system. System components include: supplemental PowerTap™ (Cat. No. 1834-SUP-PWR), gateway (Cat. No. 1834-AENTR), flat media cable (Cat. No. 1486-CBL-x), and flat media connectors (Cat. No 1486-CON-x).
  • Used within its specified ratings defined by Rockwell Automation.
  • Installed in compliance with the enclosure, mounting, spacing, and segregation requirements of the ultimate application.
  • Installed according to the instructions provided within this chapter. When this product is used in an
    EtherNet/IP
    In-cabinet system application, all system certifications apply.
  • Powered from a source compliant with Safety Extra Low Voltage (SELV) or Protected Extra Low Voltage (PELV) to comply with the CE Low Voltage Directive (LVD). Transient protection shall be provided that is set at a level not exceeding 140% of the peak-rated voltage value at the supply terminals to the equipment.
  • Disconnected from power before removal or replacement. Do not remove or replace a module while power is applied. Interruption of the flat cable media can result in unintentional operation or machine motion.
  • Route and secure the flat media cable to avoid damage. Install 0.6 mm (0.02 in.) minimum thickness insulation surrounding the flat media cable nearest the enclosure/cabinet hinge, for added protection during door closure. For example, 3M® Rubber Insulating Tape #23 or #130C, which conforms and self-fuses, serving as a jacket to envelop the flat media cable.
WARNING:
Installation Precautions
These products must only be:
  • Used as a component in an
    EtherNet/IP
    In-cabinet system. System components include: supplemental PowerTap™ (Cat. No. 1834-SUP-PWR), gateway (Cat. No. 1834-AENTR), flat media cable (Cat. No. 1486-CBL-x), and flat media connectors (Cat. No 1486-CON-x).
  • Used within its specified ratings defined by Rockwell Automation.
  • Installed in compliance with the enclosure, mounting, spacing, and segregation requirements of the ultimate application.
  • Installed according to the instructions provided within this chapter. When this product is used in an
    EtherNet/IP
    In-cabinet system application, all system certifications apply.
  • Powered from a source compliant with Safety Extra Low Voltage (SELV) or Protected Extra Low Voltage (PELV) to comply with the CE Low Voltage Directive (LVD). Transient protection shall be provided that is set at a level not exceeding 140% of the peak-rated voltage value at the supply terminals to the equipment.
  • Disconnected from power before removal or replacement. Do not remove or replace a module while power is applied. Interruption of the flat cable media can result in unintentional operation or machine motion.
  • Route and secure the flat media cable to avoid damage. Install 0.6 mm (0.02 in.) minimum thickness insulation surrounding the flat media cable nearest the enclosure/cabinet hinge, for added protection during door closure. For example, 3M® Rubber Insulating Tape #23 or #130C, which conforms and self-fuses, serving as a jacket to envelop the flat media cable.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal