Tag as Start-Stop trigger

<Tag name> is configured as either a Start trigger or Stop trigger - Are you sure you want to delete the pen?
The pen is in use. Select
No
to keep the pen, or select
Yes
to remove the pen, and then remove it from your Start Trigger/Stop Trigger configuration. Otherwise, the trend cannot be started.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal