Enter a communications driver and path manually
If a communications driver is not in the
Communications > Network Browser
communication software network topology, enter the driver and path manually.To enter a communications driver and path manually
- At the top of theCommunications > Network Browserdialog, right-click theNetwork Browsertitle bar and selectAdvanced.
- In theDriver and Path Configurationdialog, select theDriverlist and select a driver.TIP: If the current driver name appears in quotes, the device is not a running driver. Open theNetwork Browserdialog and configure the driver.
- Enter the CIP path to the desired controller, and clickOKto accept the entry.TIP: TheNetwork Browsertopology displays manually-entered driver paths after they are saved. They appear wherever the current path normally displays, with the driver and path concatenated, such as AB_KTC-1\2,6,1,0.
Provide Feedback