Failed to paste from the system clipboard
Components are protected by License Source Protection
Could not paste the item into the project because one or more components are protected by License Source Protection, which is not supported on the selected controller in this version of the
Logix Designer
application.To resolve the problem, try one of these options:
- Remove License Source Protection from the components before pasting them.
- Paste the component into a project on aControlLogix5570 orCompactLogix5370 controller.
Remote modules configured as Listen Only cannot be pasted into this controller project
Cannot import remote modules configured as
.
Listen Only
from L5K/L5X files or pasted into a project on
CompactLogix
5380, CompactLogix
5480, ControlLogix
5580, Compact GuardLogix
5380, and GuardLogix
5580 controllersTo resolve the problem, change the connection type in the
Module Definition
dialog box and import the module again.PlantPAx instructions are not supported by this controller type
Could not paste the item into the project because the item contains a PlantPAx instruction, which is not supported on the selected controller in this version of the
Logix Designer
Logix Designer
application.
TIP:
For additional information on possible causes of a pasting error, check the
Errors
tab. To open or close the Errors
tab, select View > Errors
. Provide Feedback