Applying controller name change might result in loss of privileges
When you change the name of the controller when the controller is secured by a Logical Name (the name of the controller), some users might lose privileges to view or edit the project or its components. Check the permission settings for the newly selected Logical Name in
FactoryTalk Administration Console
to make sure they provide privileges to users who need access to the project.Provide Feedback