Scroll, expand, and collapse the organizer tree
You may want to drag-and-drop an item onto another item that is hidden, either because it
is above or below the visible part of the tree in the organizer, or it is located in a
collapsed branch of the tree.
To scroll up or down in the tree | Drag the selected item to the top or the bottom of the tree window. |
To expand a collapsed branch | Drag the selected item so that the mouse pointer is over the "+" (plus icon) for the collapsed branch. |
To collapse an expanded branch | Drag the selected item so that the mouse pointer is over the "- (minus) for the expanded branch. |
Provide Feedback