Sequence Summary Control property settings
The
Sequence Detail Control
has the following properties that are configurable in the Property Panel
of the control in the FactoryTalk View SE
application.Property name | Description | Read only | Value type |
|---|---|---|---|
AutoLoad | Determines if the sequence chart is loaded automatically after the FactoryTalk View SE runtime starts. | No | Boolean |
Column1Content | Determines what content is displayed in Column 1. | No | 1 – ID 2 – State 3 – Mode 4 – Phase Failure 5 – Sequence Failure 6 – Owners 7 – Unit ID 8 – NotUsed |
Column2Content | Determines what content is displayed in Column 2. | No | 1 – ID 2 – State 3 – Mode 4 – Phase Failure 5 – Sequence Failure 6 – Owners 7 – Unit ID 8 – NotUsed |
Column3Content | Determines what content is displayed in Column 3. | No | 1 – ID 2 – State 3 – Mode 4 – Phase Failure 5 – Sequence Failure 6 – Owners 7 – Unit ID 8 – NotUsed |
Column4Content | Determines what content is displayed in Column 4. | No | 1 – ID 2 – State 3 – Mode 4 – Phase Failure 5 – Sequence Failure 6 – Owners 7 – Unit ID 8 – NotUsed |
Column5Content | Determines what content is displayed in Column 5. | No | 1 – ID 2 – State 3 – Mode 4 – Phase Failure 5 – Sequence Failure 6 – Owners 7 – Unit ID 8 – NotUsed |
Column6Content | Determines what content is displayed in Column 6. | No | 1 – ID 2 – State 3 – Mode 4 – Phase Failure 5 – Sequence Failure 6 – Owners 7 – Unit ID 8 – NotUsed |
Column7Content | Determines what content is displayed in Column 7. | No | 1 – ID 2 – State 3 – Mode 4 – Phase Failure 5 – Sequence Failure 6 – Owners 7 – Unit ID 8 – NotUsed |
CommandButtonLocation | Determines the location of the command buttons displayed. Default value: 0 – Bottom | No | 0 – Bottom 1 – Right 2 – Top 3 – Left |
ConfirmedCommands | Specifies a command group that requires confirmation when any of the command buttons in that group is pressed. Default value: 0 - None | No | 0 – None 1 – StopAndAbort 2 – All |
ControllerPath | Controller path of the Equipment Sequence . This path is specific to the workstation on which the SequenceManager Server is communicating with is located.Path example: AB_ETH-1\99.99.99.99\Backplane\0 | No | String |
ControllerShortcut | FactoryTalk Linx device shortcut to the controller. Default value: MY_CONTROLLER | No | String |
DataServerPath | The FactoryTalk View SE path to the FactoryTalk Linx Data Server.Path Example: MyProject/MyArea -or- RNA://$Local/MyProject/ | No | String |
IsEveryTagConnected | Displays whether every tag is connected to the ActiveX Control. Default value: True | Yes | Boolean |
IsLiveDataConnected | Displays whether the live data server is connected to the ActiveX Control. Default value: False | Yes | Boolean |
IsSeqMgrServerConnected | Displays whether the primary SequenceManager server is connected to the ActiveX Control. Default value: False | Yes | Boolean |
IsSeqMgrServerConnectedBackup | Displays whether the backup SequenceManager server is connected to the ActiveX Control. Default value: False | Yes | Boolean |
IsSeqMgrServerToControllerConnected | Displays whether the primary SequenceManager server is connected to the controller. Default value: False | Yes | Boolean |
IsSeqMgrServerToControllerConnectedBackup | Displays whether the backup SequenceManager server is connected to the controller. Default value: False | Yes | Boolean |
LoadTable | Determines if the table is loaded to the window. Default value: False | No | Boolean |
SelectedSequenceName | String containing the name of the currently selected Equipment Sequence . | No | String |
SelectedSequenceState | Displays the state of the selected Equipment Sequence . | Yes | String |
SeqMgrServerAddress | Displays the IP address of the computer hosting the primary SequenceManager server. | Yes | String |
SeqMgrServerAddressBackup | Displays the IP address of the computer hosting the backup SequenceManager server. | Yes | String |
SeqMgrServerPortNumber | Port number of the hosting SequenceManager server. Default value: 7452 | No | String |
ShowCommandButtons | Determines if the command buttons are shown. Default value: True | No | Boolean |
ShowStatusBar | Determines if the status icons are shown. Default value: True | No | Boolean |
SortField | An enumerated value that determines which column the table is sorted upon. Default value: 0 - Name | No | 0 - Name 1 – ID 2 – State 3 – Mode 4 – Phase Failure 5 – Sequence Failure 6 – Owners 7 – Unit ID |
TouchPointerSize | Determines the size of the command buttons and the height of the fields in the header and footer areas. | No | 0 – AutoSelect 1 – Large 2 - Small |
Provide Feedback