Overview of the Sequence Detail Control status header area
The header area of the Sequence Detail Control shows live data values for the currently loaded
Equipment Sequence
. 
Item | Name | Description |
![]() | Owners | Shows the current owner of the displayed Equipment Sequence and visual indication of ownership overrides.
|
![]() | Unit ID | Indicates the integer value currently assigned to the sequence. Configured on the Sequence Properties Dialog Box , Configuration tab, that represents the equipment unit the sequence is coordinating. |
![]() | Sequence ID | A string entered by the operator or control engineer using the Set ID button to specify an identifier for this execution of the equipment sequence. Once the sequence is executing (not in an IDLE state), the Sequence ID cannot be changed. |
![]() | State | Shows the current state of the displayed Equipment Sequence . States are:
|
![]() | Substate | Displays the state of the bits in Pause Control. The following states are:
|
![]() | Mode | Shows the current execution mode of the displayed Equipment Sequence , either Automatic or Manual . |
Provide Feedback