Monitor a step in the Sequence Detail Control
- A monitored equipment sequence step shows several functions:
- The user-configured step name and theEquipment Phasename.
- The step execution state.
- If the step is a source or target for a transfer of control.
- If the step has a failure.
- The step is executing.
- If the step or associated phase is paused.

Item | Description | |
|---|---|---|
![]() | Failure | Phase failure - generated by the Equipment Phase Failure (PFL)
instruction in the Equipment Phase logic.Internal failure - the sequencing engine has encountered a problem
with the Equipment Sequence |
![]() | Step Name
| The name of the step as configured during creation of the Equipment Sequence . |
![]() | Pause status | The symbol shows that:
|
![]() | Equipment Phase Name | Each step is configured to reference on phase. The name of the phase
is displayed so you know which equipment phase is executing. |
![]() | Transfer of Control (TOC) | A step that has been configured as the source to transfer ownership
to a following target step, without stopping the execution of the
phase. The symbol shows:
When transfer of control is not configured, the symbols are not
drawn. |
![]() | Step State | When a step is active, and attached to its phase, the step state
mirrors the state of the phase. The set of displayed states are:
INACTIVE, NOT CONNECTED (active but not attached), IDLE, RESTARTING,
RUNNING, RESETTING, HOLDING, STOPPING, ABORTING, HELD, STOPPED, ABORTED,
and COMPLETE.
TIP:
<No phase> steps have no
associated phase and only have two displayed states: RUNNING and
IDLE.
The step state is also represented by the color of the
step. |
Provide Feedback