Tools
The Tools section in the allows to access Tools and a Tools
download section:
FactoryTalk®
Remote Access™
Manager- USB device configurator
- Connection settings
- Device setup
- Download
TIP:
See FactoryTalk Remote Access Manager Tools and related sub-sections to
learn about connection settings and device setup.
USB device configurator
This section allows you to create a configuration for a device and export it to a USB
memory stick. The configuration is stored in the
.json
format. You can
only use this configuration on a new or factory-restored device. You can use the
configuration on the USB device multiple times on devices of the same type.Select the device you want to create the configuration for.
TIP:
The available devices are Optix Edge and
Stratix
4300
.The
Accounts
section is pre-selected. You must create a new password
for the administrator. Optionally you can enable a user account and create a password for
the account.In the
Interfaces
section, configure the Ethernet ports. For more
information, see your device user manual.In the
Runtime
section, select the Domain
registration
and provide the device name and select a folder where you want to
register your device. The configured device is automatically registered in the domain from
which the .json
file was generated. In the
Runtime
section you can configure a connection and local
connection.Provide Feedback