Statistics

The
Statistics
section provides a dashboard for monitoring and analyzing device statistics within the domain.
The dashboard offers insights into device
Availability status
,
System family
,
Runtime version
, and
Runtime update status
.
TIP: The Devices statistics page is accessible to admins only.
Devices statistics provides aggregated, read-only information. To view these details for individual devices and to perform device-level actions, select
Explorer
Devices view
. For further information, see Devices view.

System family

The
System family
chart shows how devices in the domain are grouped by type. Devices listed in
Explorer
Devices view
are arranged into the following categories:
System family
Description
Runtime
Generic runtime for PC (Windows, Ubuntu, Docker)
HMI
OptixPanel (Standard, Compact)
Router
All router devices (
Stratix4300
)
IIoT gateway
Embedded Edge Compute Module
OptixEdge

Availability status

The
Availability status
chart shows the proportion of devices that are currently
Online
or
Offline
.

Version

The
Version
chart summarizes the
FactoryTalk®Remote Access
runtime versions used by the devices in the domain.
The chart lists runtime versions starting from the latest version. When more than five minor versions exist for the same major runtime version, the chart groups them into a single bar by major version. When five or less minor versions exist, each minor version is displayed as its own bar.

Update status

The
Update status
chart shows the percentage of devices that are:
  • Up to date
  • Out of date
TIP: The chart includes only devices that have an update status. Devices that require a manual update and do not show any value in the
Update status
column under
Devices view
are excluded.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal