FactoryTalk®
Remote Access™
FactoryTalk®
Remote Access™
The consists of a web interface that allows you
access a domain and interact with remote devices, such as routers, HMI terminals or IPCs that
you wish to control. Furthermore, the allows you to manage domain users and their
permissions, and remote devices, including their registration, connection, setting, etc.
FactoryTalk®
Remote Access™
FactoryTalk®
Remote Access™
You need to create a user account first, then you can access
FactoryTalk®
Remote Access™
Manager.
NOTE:
See Start FactoryTalk Remote Access for further information on this subject.
Provide Feedback