Install Docker and Docker Compose
    Install Docker and Docker Compose on your host device, based on whether you have an Ubuntu 22.04 or a Debian 11.9 host device.
- Access the Install Docker Engine webpage.
- SelectUbuntuorDebian, based on the host device on which you want to install Docker.
- Install Docker Compose as a plugin by following the instructions provided at the Docker website. For example, you can follow the instructions provided at the Install using the repository webpage.
Provide Feedback