Software Updates
    SQL backups are automatically managed by Azure and geographically spread in order to minimize the possibility of data loss.
The updates can be either downloaded from the website and installed manually, or they can be installed by the Access Server semi-automatically. In the latter case, an organization admin is still responsible for manually deciding what device to update and when (immediately or within a scheduled time frame). After giving instructions to the servers via Frontend, the updates will be delivered from the cloud as planned.
A fully automatic update function without user intervention is not available for security
      reasons, because  is meant
      to be installed and used in mission-critical installations.
FactoryTalk®
          Remote Access™
Provide Feedback