Cyberattacks Countermeasures
    This section briefly describes 
      countermeasures to help protect against some common cyberattacks.
FactoryTalk®
          Remote Access™
Brute force detection
      After a few unsuccessful sign in attempts, Access Server blocks all the incoming public IP addresses for a few minutes.
This measure makes brute force JSON Web Token (JWT) attack attempts ineffective.
Code Signing
      FactoryTalk®
            Remote Access™
FactoryTalk®
            Remote Access™
Man-in-the-middle
      Access Server, Web APIs, and Frontend-Runtime connections all use end-to-end encryption (explained earlier) that make man-in-the-middle attacks not possible.
Provide Feedback