Authorization
    FactoryTalk®
          Remote Access™
The customer’s 
      organization contains all the organization resources: users, groups and devices. The
      organization administrator can design the organization and its rules to map any Rockwell
      Automation 9 Security Architecture kind of organizational structure. Specifically, new users
      and groups can be created to map the organization properly and make configuration easier and
      more scalable.
FactoryTalk®
          Remote Access™
Policies and permission rules can be applied to single resources or folders to apply them in a hierarchical way.
Finally, the Web API and the Access Server will enforce types of operations (such as remote desktop or file transfer) that will be allowed for a certain user of a certain resource (such as a remote device).
The  online
      help describes all the ways authorization rules can be configured.
FactoryTalk®
          Remote Access™
Provide Feedback