Invite users to a device
    An 
Administrator
 user of a Runtime device can invite a user that has
        a 
      account to access and use that device for a specified period.FactoryTalk®
          Remote Access™
     NOTE: 
    
The 
Administrator
 user can revoke an invitation or change its expiration date and time. See the User permissions management section to learn more about invitations management.In any case, the invited user will receive a notification email informing them about any changes.
Invite a user
      - In the or section, right click on the device.
- SelectInvite user.
- A dialog box pops up. Select the user that you wish to invite and the expiration time and date for the invitation.
- The invited user receives an email including the invitation details.
The user is able to access the Runtime device until the specified expiration date and time.
     NOTE: 
    The system monitors the remaining days until the set expiry date and time, and accordingly sends notification emails to the user.
Provide Feedback