Station Runtime (M)

This M example shows you a system architecture using an HMI and two web clients.
M System architecture
A diagram of sample system.
This example architecture has the following components:
  • Single HMI station with typical HMI functionality and three web clients
  • Communicates with multiple
    Rockwell Automation®
    controllers and multiple third-party controllers
  • Logs data to an internal database
  • Requires event logging, alarming, recipes, and basic PDF reporting
The following picture shows example runtime sizing for a package that includes these application components.
M with HMI and two web clients
An example runtime sizing for a package in a L system.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal