FactoryTalk® Optix™ Application
FactoryTalk® Optix™
ApplicationThe
FactoryTalk® Optix™
Application is the HMI or IoT
application that is developed and compiled in FactoryTalk® Optix Studio™
. The
FactoryTalk® Optix™
Application comprises two main
components:- Project - Represents the design and configuration of your application
- Runtime - The Runtime environment where your application runs
Package Components

FactoryTalk® Optix™
Application is self-contained and can
run for 2 hours full-featured on the target computer. To run the FactoryTalk® Optix™
Application in production, FactoryTalk Optix Runtime Tools is required.Application Sizing
Feature tokens function as a unit of currency and accumulate as you configure more features
in an application. Each function has a token value, some functions are free with a token
value of zero. You can upgrade your entitlement at any time to allow application expansion,
and there is an unlimited option that gives you maximum flexibility and expansion.
The selection of components and functions to be activated and used in the project is done
at the time of programming with
FactoryTalk® Optix Studio™
. FactoryTalk® Optix™
Runtime verifies that the total number
of tokens that are associated with all activated features is within the token limit of your
purchased entitlement.Each
FactoryTalk® Optix™
Runtime entitlement corresponds
to a feature token package (see Feature Tokens), within which designers
can select and activate the functions necessary to develop an application. Examples of features that affect the sizing of your application:
- Controller connections
- Multiple web clients
- Alarming
- Recipe
- PDF reports
- Data logging
- Database connectivity
- OPC UA connectivity
Provide Feedback