Access a
FactoryTalk® Hub
Application

  1. Click the appropriate panel, such as
    FactoryTalk® Design Studio
    or
    FactoryTalk® Remote Access
    , to go to that application.
  2. Click Home to return to the Home screen.
    Each application has Getting Started information in the online help to help you learn how to perform different tasks.
FactoryTalk Hub Home Page
Callout
Item
1
FactoryTalk Hub Menu.
enables navigating between different options available in the application according to the selected organization and user’s permissions. This menu also contains hub management tools if you are an owner or admin for the organization.
2
Name of the FactoryTalk Hub service you are currently using.
3
Breadcrumb that shows which organization you are currently working with. The breadcrumb changes when you switch between organizations. By clicking the arrow on the right of the parent organization, you can see and select sub-organizations you have access to. If you select a sub-organization is appears at the end of the breadcrumb after its parent organization. By clicking on the parent organization, you can return to it.
4
FactoryTalk Hub Service tiles area. Allows you to select and launch services you are entitled to use. By selecting the star on an application tile, you mark it as a favorite and the tile appears with the other favorites in the favorites row.
5
Notifications menu. Select to see notifications that have been sent to your organization since the last time you signed on. A red number here indicates the number of unread notifications that you have waiting. Click the
Notifications
icon to review the notifications list and respond to alerts.
6
Help button. Provides access to the help menu for the current application. On the main FactoryTalk Hub screen, this link goes to FactoryTalk Hub help. Otherwise to help for the application you are using. You can review the release notes, getting started information, and help topics. Use to contact support, provide feedback, or view legal information.
7
Access the profile of the current user. Select your
Profile
icon to update account settings or log out of FactoryTalk Hub.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal