Track file uploads

Configure a UI Session event to track completed file uploads in web presentation engine sessions.
Prerequisites
  1. Create a
    UISession
    #
    object by right-clicking
    UI
    and selecting
    New
    UISession
    #
    .
  2. Create a web presentation engine and associate a UI Session with the web presentation engine.
    For more information about presentation engines configuration, see Configure a web presentation engine.
  3. Implement the Upload file method into the application logic.
  1. To track file uploads
  2. In
    Project view
    , select a
    UISession
    #
    (type)
    object associated with a web presentation engine.
  3. In
    Events
    , associate a method to trigger when a file upload completes in a web presentation engine session:
    1. Next to
      UploadFileCompletedEvent
      , select
      +
      .
    2. Select and configure a method to trigger when file upload completes.
      For more information about the available methods, see #.
    For example, display a confirmation dialog when file upload completes.
    TIP: Implement handlers for upload
    Operation ID
    ,
    Result code
    , and
    File path
    in your application logic. For more information, see UploadFileCompletedEvent.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal