RA EtherNet/IP Driver compatibility

The
RA EtherNet/IP Driver
supports various Logix controller families, including
ControlLogix®
,
GuardLogix®
, and
CompactLogix®
. Compatibility depends on firmware versions and redundancy features.
  • The RA EtherNet/IP Driver supports these controller families:
    • ControlLogix®
      5560
    • GuardLogix® 5560
    • 1769-L35E and 1769-L32E
      CompactLogix®
    • 1769-L35CR
      CompactLogix®
    • 1768
      CompactLogix®
    • 1768
      Compact GuardLogix®
    • ControlLogix®
      5570
    • GuardLogix®
      5570
    • CompactLogix®
      5370
    • ControlLogix®
      5580
    • CompactLogix®
      5380
    • Compact GuardLogix®
      5370
    • GuardLogix®
      5580
    • Compact GuardLogix®
      5380
    • CompactLogix®
      5480
    • ControlLogix®
      5590
NOTE: The driver supports Logix firmware versions v20, v24, v28 and higher. However, not all controllers and controller families are supported on all versions of Logix.
NOTE:
  • 5560 Redundancy v20 supports IP Address Swapping only.
  • 5570 Redundancy v20 and greater supports IP Address Swapping only.
  • 5580 Redundancy v33 and greater supports IP Address Swapping only.
  • 5590 Redundancy v38 supports IP Address Swapping only.
You cannot use the 1756-ENET EtherNet/IP Bridge Module with the
RA EtherNet/IP Driver
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal