OPC UA
FactoryTalk Optix Studio
is compliant with the OPC UA (OPC Unified Architecture) standard and can communicate with any OPC UA client or server.
TIP:
Devices with a configured
FactoryTalk Optix Application
can operate as an OPC UA client or server.This section includes
- OPC UA server and client components, and communication between OPC UA components.
- Server setup, client setup, node import, and NodeSet import.
- Security policies, message security modes, certificates, and keys.
- Companion Specifications, localized nodes, and OPC UA methods.
- OPC UA troubleshooting, including port and certificate problems.
Components
Use these OPC UA components to develop your application logic:
- OPC UA server object. See OPC UA server.
- OPC UA client objects. See OPC UA client.
- OPC UA nodes imported from an OPC UA server or a NodeSet. See Import nodes at runtime and Import nodes from NodeSet.
Communication
Your system needs to meet the minimum security policy and message security mode to allow for communication between OPC UA components. For more information, see OPC UA communications security and OPC UA certificates and keys.
Companion Specifications
Use predefined Companion Specifications or import and export Companion Specifications. See OPC UA Companion Specifications.
Localized nodes
When an OPC UA client (see Add an OPC UA client) imports nodes from an OPC UA server (see Add an OPC UA server), any localized text variable value is imported as a translation key and not as localized text. To display the text box with text on the client device, see Add a locale language to a localization dictionary and import the localization dictionary from the server. For non-FTOptix servers, use the
Connection Locale ID
property of the OPC UA client. The client then connects using that locale ID and the server sends the value of localized text variables as localized texts with that locale ID.In addition to importing the localization dictionary, you must specify a locale to the
Localization/Locales
property, add a new user with the Language property set to the locale, and then specify that user as the starting user in the native presentation engine object. OPC UA methods
OPC UA methods are callable functions that interact with backend logic. OPC UA methods can
execute commands, retrieve data, or trigger operations. Use OPC UA methods to control
devices, perform calculations, or manage workflows.
To leverage existing OPC UA methods by:
- Import nodes from an OPC UA server. See Synchronize the imported nodes at design time and #.
- Import nodes from NodeSet. See Import nodes from NodeSet.
- ImportCompanion Specifications. See Import Companion Specifications.
Develop custom OPC UA methods in NetLogics using C#. For more information, see NetLogic and Define methods in C#.
To integrate OPC UA methods into the
FactoryTalk Optix Application
logic, see Read output values of a method.opc ua
unified architecture
Provide Feedback