Model change events
Model change event types, generators, triggers, and use cases for
FactoryTalk Optix Applications
.Event type | Generator | Trigger | Use cases | Examples |
|---|---|---|---|---|
BaseModelChangeEventType | EventManager | Base type for all model change events | Comprehensive model modification tracking | Node, reference, or attribute changes trigger base event |
GeneralModelChangeEventType | EventManager | General model structure changes occur |
|
|
AttributeChangesEvent | EventManager | Node attributes change (browse name, display name, description,
valueRank) |
|
|
ReferencesAddedEvent | EventManager | Reference created between nodes |
| New "HasAlarm" reference added to variable |
ReferencesRemovedEvent | EventManager | Reference deleted between nodes |
| "HasAlarm" reference removed from retired variable |
NodesAttachedEvent | EventManager | Node added to parent |
| New alarm object attached to Process folder |
NodesDetached Event | EventManager | Node removed from parent |
| Test alarm deleted from system |
SemanticChangeEventType | EventManager | Semantic meaning of model changes |
| Variable redefined from process value to reference |
RefreshStartEventType | EventManager | Subscription refresh begins |
| Client subscription refresh started |
RefreshEndEventType | EventManager | Subscription refresh completes |
| Full model snapshot transmitted to client |
event
audit
OPC UA
Provide Feedback