Develop a button that animates an SVG image
Configure an Advanced SVG Image object to animate the image at runtime.
NOTE:
Download a sample project:
RotateImage.zipApplication example

Provide Feedback