Develop a button that replaces an SVG image

Create a button and NetLogic that modifies an SVG image at runtime.
NOTE:
Download a sample project:
ReplaceImage.zip
Application example
Application window with a large dark blue star and a smaller orange square, plus a
          button labeled Replace image.
Prerequisites
#.
Large blue star and small orange square inside a bordered area, with an unlocked
            padlock icon above and a Replace image button to the right.
Select
Run icon
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see #.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal