Create a certificate
To communicate securely, OPC UA applications must have appropriate public certificates and corresponding private keys.
Certificates created in
FactoryTalk Optix Studio
are self-signed. To use such
certificates, you need to set OPC UA clients to trust these certificates.
IMPORTANT:
Do
not
use self-signed certificates in
production environments.Alternatively, generate self-signed certificates and certificates trusted by Certificate
Authorities (CA) in third party tools.
IMPORTANT:
Rockwell Automation
is not responsible for any third-party software, including but not limited to its
performance, security, updates, or compatibility with our products. Any use of third-party
software is at your own risk, and we do not provide support, warranties, or guarantees for
such software. Users should refer to the respective third-party providers for assistance and
licensing terms.- In the title bar, select the drop-down arrow afterand select
FactoryTalk Optix Studio OptionsCreate certificate. - UnderSubject, complete:
- Common name. Name of the OPC UA application.
- Organization. Registration name of the company responsible for the certificate. Do not use non-alphanumerical characters or abbreviations.
- Organization unit. Division in your organization responsible for the certificate.
- Locality. City where your organization or organization unit is located. Use proper location names, as specified in the postal address. Do not use abbreviations.
- State. Geographical area where your organization or organization unit is located. Geographical areas include states and provinces.
- Country. Two-letter ISO-3166 country code where your organization or organization unit is located. For example,IT.
- UnderOPC UA information, complete:
- Application URI. Unique identifier for the project on a specific machine. Must be the same as theProduct URIin the server configuration. See #.
- Domain names. Local and remote domain names that you can use to access the machine.IMPORTANT: DNS names are only recognized if they are lower case.
- IP addresses. (optional) IP addresses that you can use to access the machine.
- UnderCertificate settings, complete:
- RSA key strength. The size, in bits, of the RSA key.IMPORTANT:TheRSA key strengthandSignature algorithmvalues are compatible with the OPC UA security policies that you set in the OPC UA server and OPC UA client objects.The higher theRSA key strengthandSignature algorithmvalues, the greater the use of resources for the encryption and decryption of messages between the server and client.
- Signature algorithm. Algorithm used by devices to sign data with the certificate.
- Expiration date. Determines for how long the certificate will be valid.
- InName, enter a file name for the certificate.
- InLocation, enter or browse to the location to store the certificate.
- SelectCreate.
Rockwell Automation
recommends backing up the certificate to a personal
folder outside of the project.certificate
Provide Feedback