Configure a custom keyboard

Configure a custom virtual keyboard by adding a Keyboard object and adjusting its children objects and properties.
Prerequisites
Select the custom virtual keyboard engine by setting
Virtual keyboard
to
Custom
. See Configure a native presentation engine and Configure a web presentation engine.
  1. To configure a custom keyboard
  2. In
    Project view
    , expand
    UI
    , right-click
    Keyboards
    and select
    Keyboard
    .
    TIP: You can import a predefined keyboard from template libraries if you do not want to add all keyboard keys from scratch. You can modify the imported keyboard at any point. For more information, see Import a template.
  3. In
    Properties
    , set keyboard options:
    • Locales
      . Locales for which to use this virtual keyboard. For more information, see UI session.
      TIP: If you do not specify a custom keyboard for the current locale, FactoryTalk Optix uses the first available keyboard following the
      Locales fallback
      property of the project object.
    • Keyboard type
      .
      Alphanumeric
      ,
      Numeric
      or a custom keyboard type.
      For example, set
      Keyboard type
      to
      CustomKeyboard
    • Preedit control
      . Dynamic link to a graphic object that displays the text to be applied after editing is complete. For example, a dynamic link to a text box.
      For more information about dynamic links, see #.
  4. In
    Project view
    , to add keyboard keys, right-click the keyboard and select either:
    • Keyboard text button
      and then, in
      Properties
      , enter a character in
      Key
      .
      For example, in
      Key
      , enter
      q
      .
      TIP:
      The characters are automatically uppercase or lowercase based on the
      ShiftActive
      property value of the Shift keyboard key. You can also use the
      ShiftActive
      value in your application logic.
      You cannot use emoticons for
      Key
      characters.
    • Keyboard symbol button
      and then, in
      Properties
      , select a symbol.
      For example, select
      Enter
      or
      Change sign
      from
      Symbol
      .
  5. (optional) In
    Properties
    , modify the
    Size and layout
    and
    Appearance
    properties of the keyboard.
  6. (optional) In
    Project view
    , expand the keyboard object and manage the children objects.
    For example, you can:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal