Configure the trusted certificates at design time
Set up a trusted certificate at design time by importing a file that has the
certificate.
TIP:
This configures application transport trust. To configure
certificate user login, see Configure certificate user login.
- From the toolbar, select.
Browse project files - Select a certificate and select.
Import file(s) - Select the certificate.For more information, see #.
- SelectClose.
Provide Feedback