Configure a range transitioned event

Trigger methods if the value of a variable or object property is in or out of a specific range.
  1. In
    Project view
    , select an object or a variable.
  2. In
    Properties
    , right-click a variable or a property and select
    New
    Range transitioned event
    .
    TIP: If needed, select
    Add icon in black
    to add a variable.
  3. In
    Events
    , from
    Transition
    select:
    • In (Exclusive)
      Graph showing an exclusive In range event with arrows indicating entry
                    between two open circles on a number line.
    • Out (Exclusive)
      Graph showing an exclusive Out range event with arrows indicating exit
                    between two open circles on a number line.
    • In (Inclusive)
      Graph showing an inclusive In range event with arrows indicating entry
                    between two filled circles on a number line.
    • Out (Inclusive)
      Graph showing an inclusive Out range event with arrows indicating exit
                    between two filled circles on a number line.
    Item
    Description
    A
    Range
    B
    Value transition
    C
    Method execution
  4. Set the
    From
    property.
    TIP: You can enter the threshold value or add a dynamic link to the threshold value. For more information about dynamic links, see #.
  5. Set the
    To
    property.
    TIP: You can enter the threshold value or add a dynamic link to the threshold value. For more information about dynamic links, see #.
  6. Next to
    VariableTransitioned
    , select
    Add icon in black
    .
  7. Select a method:
    • For global methods, expand
      Commands
      .
    • For local methods, expand the nodes that expose methods (for example, a
      DataGrid
      node exposes a
      Refresh
      method), or expand the node related to a specific NetLogic.
  8. (optional) If the method requires arguments, expand the method and set arguments.
  9. (optional) Select additional methods.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal