Audit events

Audit event types, generators, triggers, and use cases for
FactoryTalk Optix Applications
.
Event types
Event type
Generator
Trigger
Use cases
Examples
AuditAddNodesEventType
AuditEventEmitter
New node created in information model
  • Audit trail for model changes
  • Compliance logging
  • Change management
  • Create a variable
  • Instantiate an alarm object
  • Add a method
AuditAddReferencesEventType
AuditEventEmitter
Reference created between nodes
  • Model relationship tracking
  • Dependency auditing
New "HasComponent" reference linking pump to tank
AuditDeleteNodesEventType
AuditEventEmitter
Node deleted from information model
  • Model cleanup
  • Feature removal
  • Compliance documentation
Temporary variable removed after test phase
AuditDeleteReferencesEventType
AuditEventEmitter
Reference between nodes deleted
  • Model simplification
  • Relationship removal
Tank-to-pump connection removed
AuditEventType
AuditEventEmitter
Base event type for all audit operations
  • Comprehensive system audit trail
  • Compliance logging
Any audit-level operation (node management, variable changes, method calls, object updates)
AuditNodeManagementEventType
AuditEventEmitter
Nodes added or deleted
  • Model structure auditing
  • Change management
  • Variable creates during runtime
  • Alarm deletes
AuditUpdateEventType
AuditEventEmitter
OPC UA objects updated
  • Object change auditing
  • Configuration updates
  • Object properties changed
  • Object state updated
AuditUpdateMethodEvent
AuditEventEmitter
Method called on object
  • Action tracking
  • Workflow auditing
  • Start()
    method called on pump controller
  • EmergencyStop()
    method invoked
AuditWriteUpdateEventType
AuditEventEmitter
Variable values changed AND session context exists (external write)
  • OPC UA audit trail
  • Compliance logging
  • External parameter change tracking
  • High-limit setpoint written via OPC UA client
  • Operator changes PID gain
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal