Add a Station Connection Status widget

Add a Station Connection Status widget to monitor the controller connection status.
  1. To add a Station Connection Status widget
  2. From the main toolbar, select
    Template Libraries icon
    Template Libraries
    .
  3. In
    Libraries
    , search for
    Station Connection Status
    .
  4. Under
    Components
    , drag
    Station Connection Status
    to
    MainWindow (type)
    or a different UI container in
    Project view
    .
  5. In
    Properties
    , create a dynamic link between
    Station
    and the communication driver station that you want to monitor.
    For more information about dynamic links, see #.
At runtime, the widget displays these LED status indicators:
  • Green LED
    . Connected to the controller.
  • Red LED
    . Disconnected from the controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal