Deployment and compatibility FAQs

Find answers to common questions about deploying
FactoryTalk Optix Applications
, compatibility with devices, intellectual property protection, and upgrade or downgrade options.

How do I deploy a FactoryTalk Optix Application?

Deploy a FactoryTalk Optix Application from FactoryTalk Optix Studio. See Deploy a FactoryTalk Optix application.

Can I deploy a FactoryTalk Optix Application to a device that is running a previous version of FactoryTalk Optix Runtime?

Yes, the Runtime version updates when you deploy the FactoryTalk Optix Application. See Deploy a FactoryTalk Optix application.

What happens when I deploy a FactoryTalk Optix Application to an Optix Panel that already has an application deployed?

The OptixPanel can have only one FactoryTalk Optix Application at a time. If you have deployed ProjectA and want to deploy ProjectB, the system will replace ProjectA with ProjectB.
If you have deployed ProjectA and want to update the project, the system will ask whether you want to update the project, which does not cause a loss of internal data, or whether you want to replace the project, which erases all internal data.
TIP: FactoryTalk Optix Studio treats projects with different names as separate projects. If you deploy ProjectA and then attempt to deploy ProjectA_updated, ProjectA will be replaced.

Is it possible to deploy a FactoryTalk Optix Application in a manner that protects intellectual property?

Yes, you can deploy a FactoryTalk Optix Application in a secure manner. See Project obfuscation on a target device.

Can I upgrade or downgrade FactoryTalk Optix Applications?

You cannot downgrade a FactoryTalk Optix Application, but you can upgrade an application. To upgrade a FactoryTalk Optix Applicatoin, upgrade the project and then redeploy the applications to the target device. See:

Can I deploy a FactoryTalk Optix Application on third-party iPC?

Yes, you can deploy and run FactoryTalk Optix Applications to third-party iPCs if the target devices satisfy FactoryTalk Optix software and hardware requirements. See FactoryTalk Optix Release Notes | System requirements.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal