Docker parameters
Reference information for Docker run parameters used to start
FactoryTalk®
Optix™ Runtime
containers with online or offline
entitlements.Parameter | Importance | Description |
|---|---|---|
--publish 49100:49100 | Required | Maps the deployment and update service port. External port 49100 must
map to internal port 49100. Do not map this service to a different
external port. |
--env
ADMIN_PASSWORD= admin_password | Required | Sets the administrator password that the container requires at
startup. |
--name container_name | Recommended | The name for the Docker container to
run. |
--publish
external_port :internal_port | Optional | Maps the web interface port from port 49100. Use this parameter if
the application uses a web presentation engine.
|
--restart unless-stopped | Recommended | Restarts the container automatically after a failure or host restart,
or if the FactoryTalk Optix Application Update Service stops
working. |
-d | Optional | Runs the container in the background. |
-v
local_folder :/root/FTOptixApplication/Projects/app_name | Optional | Binds the application folder to a local folder to persist changes
made at FactoryTalk Optix Application runtime.
|
image_name | Required | Name of the Docker image to run in the
Docker container.
TIP:
You can check the available
Docker images by entering
docker images in the terminal. |
Parameter | Importance | Description |
|---|---|---|
--env
FTOPTIX_ENTITLEMENT_SERIAL_NUMBER= entitlement_serial_number | Required | Passes the entitlement serial number to the container when you start
the container. Use this environment variable for online entitlement
validation. |
Parameter | Importance | Description |
|---|---|---|
--env
license_environment_variable =offline_entitlement_value | Required | Pass the offline entitlement value as an environment variable when
you start the container. Use the offline entitlement value for the
offline entitlement activated on the host. |
Docker runtime
Docker parameters
container licensing
online licensing
offline licensing
Provide Feedback