View alarms in standard time zone
Display alarm events in the standard UTC time zone by configuring the grid object in
Template Libraries
.- Select.Template Libraries
- InTemplate Libraries, selectWidgets.
- DragAlarm gridorAlarm history gridfromWidgetsto the desired node in theUIfolder.
- InTemplate Libraries, selectClose.
- InProject view, expand the alarm grid and selectAlarmsDataGrid.
- InProperties, expandTimestamp.
- In theTextproperty, right-clickComplex Dynamic Linkand then selectReset value.
- Select.
Change Dynamic Link - In the Dynamic Links window, configure either:
- ForAlarm Grid: ExpandAliases, select , and then select theTimevariable.
- ForAlarm History Grid: ExpandAliases, select ,and selectLocalTime. AfterLocalTime, selectand type
Time.
- ChooseSelect.
alarm grid
UTC time zone
alarm history grid
Provide Feedback