View alarms in remote local time zone

View alarms in the local time zone to view alarm events remotely.
  1. Select
    Template Libraries icon
    Template Libraries
    .
  2. In
    Template Libraries
    , drag the
    Alarm grid
    or
    Alarm history grid
    object from
    Widgets
    into a node in the
    UI
    folder.
  3. In
    Project view
    , select the alarm object.
  4. In
    Properties
    , expand
    Timestamp
    .
  5. In
    Text
    , clear the current value and then select
    Change Dynamic Link icon
    Change Dynamic Link
    .
  6. At the bottom of the window, select
    Advanced
    .
  7. In the Advanced Dynamic Link editor, select
    Insert
    and then select
    Expression evaluator
    .
  8. In
    Expression
    , enter
    {0} + {1}
  9. In the
    {0} DynamicLink
    pane, select
    Change Dynamic Link icon
    Change Dynamic Link
    and then select
    Alias
    {Item} […]
    AlarmCondition
    Time
    .
  10. In
    {1} DynamicLink
    , select
    Change Dynamic Link icon
    Change Dynamic Link
    and then select
    Alias
    {Session}
    Session
    Time Zone Offset
    .
  11. Select
    Select
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal