Customize standard units of measure
Customize measurement units at the project level to use different measurement systems for each desired quantity.
- InProject view, select the project root node.
- InProperties, afterMeasurement systems map, select
Edit with Measurement system editor. - In the title bar of theMeasurementSystemMapthat opens in the center of the screen, selectto add a new row to the map table.

- In theFromcolumn, select the input quantity of interest or the value from the sensor.The selected units of measure will be translated to the equivalent quantity for the different locales in the three remaining columns.
- In theInternational System of Units,US Customary Measurement System, andBritish Imperial Units columns, select the desired target measurement units.
Measurement units are customized for each quantity and locale in the project.
measurement units
locale
project settings
Provide Feedback