Track file uploads
Configure a UI Session event to track completed file uploads in web presentation engine sessions.
Prerequisites
- Create aUISessionobject by right-clicking#UIand selecting .
- Create a web presentation engine and associate a UI Session with the web presentation engine.For more information about presentation engines configuration, see Configure a web presentation engine.
- Implement the Upload file method into the application logic.For more information, see Method: Upload file and Add a method to an existing event.
- To track file uploads
- InProject view, select aUISessionobject associated with a web presentation engine.#(type)
- InEvents, associate a method to trigger when a file upload completes in a web presentation engine session:
- Next toUploadFileCompletedEvent, select+.
- Select and configure a method to trigger when file upload completes.For more information about the available methods, see Methods.
For example, display a confirmation dialog when file upload completes.TIP: Implement handlers for uploadOperation ID,Result code, andFile pathin your application logic. For more information, see UploadFileCompletedEvent.
Provide Feedback