Track file downloads

Configure a UI Session event to track started file downloads in web presentation engine sessions.
Prerequisites
  1. Create a
    UISession
    #
    object by right-clicking
    UI
    and selecting
    New
    UISession
    #
    .
  2. Create a web presentation engine and associate a UI Session with the web presentation engine.
    For more information about presentation engines configuration, see Configure a web presentation engine.
  3. Implement the Download file method into the application logic.
  1. To track file downloads
  2. In
    Project view
    , select a
    UISession
    #
    (type)
    object associated with a web presentation engine.
  3. In
    Events
    , associate a method to trigger when a file download starts in a web presentation engine session:
    1. Next to
      DownloadFileStartedEvent
      , select
      +
      .
    2. Select and configure method to trigger when file download starts.
      For more information about the available methods, see Methods.
    For example, display a confirmation dialog when file download starts.
    TIP: You can also implement handlers for download
    Operation ID
    and
    Result
    codes into your application logic. For more information, see DownloadFileStartedEvent.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal