Create a project template
Create a project template to contain the default content for projects that are based
on the template. Create the template from an existing project. New projects that you create
based on the template contain the content of the template by default.
- Add the content that you want to appear as default content in projects that you create with the template.
- From the toolbar, select the down arrow afterand selectSaveSave As.
- InSave project as, complete:
- Name. Enter the new name of the project.
- Location. Type the path where you want to save the project. Select and browse a folder to navigate to the location.
- Template. Select to save the project as a template.
- (optional)Use Version Control. Select to track changes made to the project and store the project in a Git repository.
- (optional)Encrypt secrets. Select to encrypt sensitive data contained in projects.
- SelectOK.
- (optional) On the Start page, in the top left corner of the newly created template tile, to add the template to favorites select.

Provide Feedback