Delete an event

Delete an external event, change event, transitioned event, or range transitioned event from an object.
TIP: You cannot delete predefined events from objects. For example, you cannot delete the MouseClick event from a button object.
  1. In
    Project view
    , select an object with the event to delete.
  2. In
    Events
    , select the event to delete.
  3. Press the
    keyboard key.
The event and all associated methods are deleted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal