UI objects
Effective UI object naming and layout practices improve readability,
maintainability, and performance. This section outlines conventions for naming,
organizing, and designing UI elements to ensure clarity and consistency.
Name a UI object
Instead of using role-based prefixes, try to keep UI object names minimal, clear, and
meaningful while avoiding redundancy.
- Use concise, descriptive names that define the object function without unnecessary prefixes. For example:
- StartActioninstead ofbtnStart
- TemperatureStringinstead oflblTemperature
- Usernameinstead oftxtUsername
IMPORTANT:
Avoid vague names like
Object1
or UIElement
.Containers and hierarchy
Containers and objects organization is essential for a collaborative environment and
to save time while creating your project.
- Organize UI objects by function using containers, such as panels, buttons, labels, graphs, and related elements.
- Use nested hierarchies for better structure and scalability.
- Minimize node count by avoiding redundant properties.
- Reduce unnecessary dynamic links that are only needed at design time.TIP: See Dynamic links for further information on this subject.
Sizing and layout
Ensure consistency in objects size and positioning for a more balanced layout in your
application.
- Ensure consistent sizing for similar UI objects.TIP: See Graphic objects layout for further information on this subject.
- Use relative positioning (anchors) to support different screen sizes.
- If you want your widgets to automatically adapt to content changes, such as font size, use the sizeAutofeature.TIP: TheAutofeature is designed for fit-to-content scenarios, making it ideal when containers need to adjust to their content or when text needs to adapt to container dimensions.To activateAuto, open thePropertiespanel and remove the value from either theHeightorWidthfield. Once cleared, the field will automatically switch toAuto, enabling dynamic resizing based on content.
Consistent design
Apply consistency for a well-finished application.
- Use style sheets and their predefined styles.
- Follow a unified theme for colors, fonts, and borders.
- Align UI elements for a structured and professional look.
TIP:
Refer to Graphic objects, Style sheets and Apply a global style to the project for further information.
Reusable Types
Use reusable types and global styles to ensure consistency and simplify maintenance
across UI components.
- Create reusable types for common UI objects, such as buttons and text fields.
- Use global styles for text and buttons to maintain uniformity.
Spacing, alignment, and grid system
Apply consistent spacing and layout alignment to create a clean, scalable, and
visually balanced UI layout.
- Follow the 8-pixel rule: Keep spacing and margins in increments of 8px (8px, 16px, 24px).
- Use a grid-based layout for better UI structure.
- Ensure consistent padding and margins for a uniform look.
Provide Feedback