Roles and Permissions
    The following table illustrates how the 
    
FactoryTalk Hub
 roles, FactoryTalk Energy Manager
 roles, and FactoryTalk DataMosaix
 roles are mapped to each other, providing a clear understanding of user permissions across different platforms:
      
  FactoryTalk Hub  | FactoryTalk DataMosaix  | FactoryTalk Energy Manager  | 
|---|---|---|
FactoryTalk Energy Manager  Service Role Administrator | Project Admin FTEM-Editor (Recommended) Data Scientist (Old Role)  |  Admin  | 
FactoryTalk Energy Manager  Service Role Contributor | FTEM-Reader  | Reader (Default)  | 
FTEM-Editor  | Editor  | 
     IMPORTANT: 
    
For the existing users, it is highly recommended to change from the 
Data Scientist
 role to the FTEM-Editor
 for a better user experience and accessibility.FactoryTalk Energy Manager
 has three predefined user roles for managing user access, each with different levels of permissions:- Admin:
- The role has full access to the entire application, includingUser Management.
 - They can modify user roles for other users such as FTEM-Editor/FTEM-Reader, but not the other admin role.
 - Admin role can be changed only inFactoryTalk Hub.
 
 - Editor:
- The role has all the permissions of the Administrator except forUser Management.
 - They can perform all operations within the application except for managing user permissions.
 
 - Reader:
- The role has read-only access to the entire application (including data/reports export).
 
FactoryTalk Energy ManagerUser Management
 
The following table details the permissions available for each role (Reader, Editor, Administrator) in 
FactoryTalk Energy Manager
. It describes the capabilities each user role has in the system:Functionality  | Reader  | Editor  | Administrator  | 
|---|---|---|---|
View Dashboard  | Yes  | Yes  | Yes  | 
Export CSV Data  | Yes  | Yes  | Yes  | 
View Tag Mapping  | Yes  | Yes  | Yes  | 
View Enterprise Configuration  | Yes  | Yes  | Yes  | 
View Resource Type Configuration  | Yes  | Yes  | Yes  | 
View Parameter Configuration  | Yes  | Yes  | Yes  | 
View Rate Schedules Configuration  | Yes  | Yes  | Yes  | 
View Emission Facto Configuration  | Yes  | Yes  | Yes  | 
View Measurand Configuration  | Yes  | Yes  | Yes  | 
View Notifications Configuration  | Yes  | Yes  | Yes  | 
View Node Summary Details  | Yes  | Yes  | Yes  | 
View Notifications  | Yes  | Yes  | Yes  | 
View Reports Configuration  | Yes  | Yes  | Yes  | 
Download Reports  | Yes  | Yes  | Yes  | 
Edit Dashboard (hide or show widgets)  | Yes  | Yes  | Yes  | 
Edit Enterprise Configuration  | No  | Yes  | Yes  | 
Add/ Edit/Delete Resource Type Configuration  | No  | Yes  | Yes  | 
Edit Parameter Configuration  | No  | Yes  | Yes  | 
Add/Edit/Delete Rate Schedules Configuration  | No  | Yes  | Yes  | 
Add/Edit/Delete Emissions Factor Configuration  | No  | Yes  | Yes  | 
Edit Measurand Configuration  | No  | Yes  | Yes  | 
Add/Edit/Delete Notifications Configuration  | No  | Yes  | Yes  | 
Add/Edit/Delete Reports Configuration  | No  | Yes  | Yes  | 
Add/Edit/Delete Meters  | No  | Yes  | Yes  | 
Configure Energy Model (Add/Edit/Delete Nodes)  | No  | Yes  | Yes  | 
Configure Data Link for Meters  | No  | Yes  | Yes  | 
User Management  | No  | No  | Yes  | 
Add/Edit/Delete Analytics Baseline models  | No  | Yes  | Yes  | 
View Analytics Baseline calculator  | Yes  | Yes  | Yes  | 
Create/Edit/Download M&V Projects  | No  | Yes  | Yes  | 
View M&V Projects  | Yes  | Yes  | Yes  | 
Provide Feedback