Onboarding A New User
    To onboard a user to 
FactoryTalk Energy Manager
, User should have access to the FactoryTalk Energy Manager
 service and FactoryTalk DataMosaix
 service. FTEM-Editor role should be assigned in the FactoryTalk DataMosaix
.
     IMPORTANT: 
    
For the existing users, it is highly recommended to change from the 
Data Scientist
 role to the FTEM-Editor
 for a better user experience and accessibility.
     IMPORTANT: 
    
- FactoryTalk Energy Managerservice-level role andFactoryTalk DataMosaixFTEM-Editor role are required for any new user to access theFactoryTalk Energy Managerapplication.
 - Users already havingFactoryTalk Huborganization-level roles can access theFactoryTalk Energy Managerapplication, but they cannot perform any changes in the user management section ofFactoryTalk Hubuntil or unless they are assigned theFactoryTalk Energy Manager–FactoryTalk DataMosaixservice-level roles.
 - If the user has an organization-level role and theFactoryTalk Energy Managerservice-level role, still they require theFactoryTalk DataMosaixFTEM-Editor role to access theFactoryTalk Energy Managerapplication.
 
Provide Feedback