Initial Setup
    For the first time, users must choose a cluster in the 
FactoryTalk DataMosaix
 application to create the Project for the FactoryTalk Energy Manager
 application.Perform the following steps to create a Project in the 
FactoryTalk Energy Manager
 application:- After a successful login for the first time, the following window displays, which navigates to theFactoryTalk DataMosaixapplication to create a project.FactoryTalk Energy ManagerDashboard

 - ClickCreate CDF Projectto go to theFactoryTalk DataMosaixSaaS application. The Initial Setup window is displayed.Initial Setup

 - Choose a cluster for your project from the available list in the drop-down.
 - Select theI understand that once a project is created, the cluster choice cannot be changed latercheck box and clickStart.The application creates the Project, and a success message is displayed as shown in the following image:Start Setup
The application might take time to create the project.Initializing
 - Go to theFactoryTalk Hubapplication and then navigate to theFactoryTalk Energy Managerapplication.The application might take time to set up your configurations.Initial Setup
Once the setup is done, the application navigates you to the Configuration page to create the Energy Model hierarchy.Create Energy Model Hierarchy
 - To create the Energy Model hierarchy, refer to the Add Enterprise Node section.
 
Provide Feedback