Copy and Paste Component
    Perform the following steps to copy and paste the component in the hierarchy list:
- Select the required component.
 - Click the [
] icon and click
Copy.NOTE:If the user copies the parent component directly, they need to selectwith childorwithout childradio button in theCopy Componentdialog and clickCopy.Copy Component
The "Component copied successfully" message is displayed. - Select the required hierarchy component to paste the copied component.
 - Click the [
] icon and click
Paste. - In thePaste Hierarchy Componentdialog box, clickPaste.Paste Hierarchy Component
The "Component pasted under component successfully" message is displayed. 
Provide Feedback