Region Level Dashboard
    Focuses on energy usage and efficiency within a specific geographical region. It consolidates data from multiple sites within the region, allowing for regional comparisons and targeted energy management strategies.
Click 
Region
 from the hierarchy list.The following table provides the list of charts available by default in the dashboard:
S.No  | Chart/Widget Name  | Description  | 
|---|---|---|
1  | Total Consumption (Harmonized)  | This is the overall summary of the total energy consumption.  | 
2  | Total Costs (Harmonized)  | This is the overall summary of the total cost.  | 
3  | Total Emissions (Harmonized)  | This is the overall summary of the resource emission.  | 
4  | Total Energy Consumption by Site chart  | The user can view the site details on the X-axis and harmonized consumption on the Y-axis. This chart shows the overall energy consumption summary.  | 
5  | Total Production by Site (by Site-wise)  | This chart shows the overall production summary site-wise.  | 
6  | Total Energy Costs by Site   | The user can view the site details on the X-axis and the cost on the Y-axis. This chart shows the overall energy cost site-wise.  | 
7  | Total Emissions by Site (All Sites)  | The user can view the site details on the X-axis and the emission on the Y-axis. This chart shows the overall emissions site-wise.  | 
8  | Total Energy Intensity by Site   | The user can view the site details on the X-axis and energy intensity on the Y-axis. This chart shows the overall energy intensity summary site-wise.  | 
9  | Top 5   | The user can view the resource details on the X-axis and attributes (Consumption, Cost, Emission) on the Y-axis. This chart shows the top 5 resources based on consumption, cost, and emission.  | 
Refer to Dashboard Features section to manage the Region-Level dashboard. 
Related Information
:Provide Feedback