Process Value Meter Dashboard
    Provides insights into various process parameters. This information contextualizes energy data within specific process values, facilitating targeted energy-saving actions and process optimization. By correlating energy consumption with process metrics, managers can identify inefficiencies, implement corrective measures, and enhance overall process performance.
Click a Process value meter from the hierarchy list.
The following table provides the list of charts available by default in the dashboard:
S.No  | Chart Type  | Description  | 
|---|---|---|
1  | Energy Details (Harmonized)  | This chart shows the maximum, minimum, and average values along with the last value and last updated time.  | 
2  | Trend   | The user can view the selected time period with the respective granularity on the X-axis and on the Y-axis, the user can view attributes (Temperature, wind, humidity, and so on). This chart shows the process value summary.  | 
Related Information
:Provide Feedback