Area/Work Center Level Dashboard 
    The Area Level dashboard provides insights into energy usage within specific areas of a site. It helps area managers track energy performance, identify high-consumption zones, and implement localized energy-saving initiatives. The Work Center Level dashboard focuses on energy consumption and efficiency within specific work centers. This level allows for detailed monitoring of energy usage in production or operational units, helping managers optimize processes and reduce energy waste.
Click 
Area
, or Work center
 from the hierarchy list.The following table provides the list of charts available by default in the dashboard under tab:
S.No  | Chart/Widget Name  | Description  | 
|---|---|---|
1  | Resources  | Consumption: This is the overall summary of the total energy consumption, with the values of each resource type. Cost: This is the overall summary of the total cost with the values of each resource type. Emission: This is the overall summary of the resource emission, with the values of each resource type.  Below, the pie chart displays the top 3 resource types by default.  A list of resource types is displayed on clicking the expand icon in the top left corner of the widget. In the expanded view, all the records are listed.  | 
2  | Total Energy Consumption (Harmonized)  | This shows the overall energy consumption summary.  | 
3  | Energy Consumption by Resource Type chart  | The user can view the selected time period with the respective granularity on the X-axis and consumption on the Y-axis. This chart shows the overall energy consumption summary.  | 
4  | Total Emissions (Harmonized)  | This shows the overall emission summary.  | 
5  | Emissions   | The user can view the selected time period with the respective granularity on the X-axis and emissions on the Y-axis. This chart shows the overall emission summary.  | 
6  | Total Production (Harmonized)  | This shows the overall production summary.  | 
7  | Production Data   | The user can view the selected time period with the respective granularity on the X-axis and production data on the Y-axis. This chart shows the overall production summary.  | 
8  | Total Energy Intensity (Harmonized)  | This shows the overall energy intensity summary.  | 
9  | Energy Intensity   | The user can view the selected time period with the respective granularity on the X-axis and energy intensity on the primary Y-axis, production data on the secondary Y-axis. This chart shows the overall energy intensity summary with the comparison of production data.  | 
10  | Total Costs (Harmonized)  | This shows the overall energy cost summary.  | 
11  | Costs   | The user can view the selected time period with the respective granularity on the X-axis and cost on the Y-axis. This chart shows the overall energy cost summary.  | 
12  | Total Consumption - Production Data   | The user can view the selected time period with the respective granularity on the X-axis and consumption in the primary Y-axis, and production data in the secondary Y-axis. This chart shows the overall consumption summary with the comparison of production data.  | 
13  | Electricity Demand Summary (Harmonized)  | This shows the overall electricity demand.  | 
14  | Electricity Demand  | The user can view the selected time period with the respective granularity on the X-axis and electricity demand details on the Y-axis. This chart shows the overall electricity demand.  | 
15  | Natural Gas Demand Summary (Harmonized)  | This shows the overall natural gas demand.  | 
16  | Natural Gas Demand   | The user can view the selected time period with the respective granularity on the X-axis and natural gas demand details on the Y-axis. This chart shows the overall natural gas demand.  | 
17  | Total Consumption (Harmonized)  | This shows the overall energy consumption.  | 
18  | Energy Consumption   | The X-axis and Y-axis granularity values are represented based on your time period selection. This chart shows the overall consumption summary in the heat map format with color representation.  | 
Refer to Dashboard Features section to manage the Area/Work Center-Level dashboard. 
Related Information
Provide Feedback